PLC Designer

The Lenze PLC Designer is the central engineering tool for programming and commissioning Lenze controllers (PLC). It supports standard-compliant IEC 61131-3 programming with several editors, integrated debugger and monitoring functions and is used for logic and motion applications. The PLC Designer is based on the CODESYS system, has been qualified and expanded by Lenze for industrial use and is closely integrated into the Lenze engineering ecosystem.

Content: