Set as start project
If a project folder (top node in the project explorer, *.sln file) contains several projects with a user interface (e.g. Single, Client), the project added first is automatically the start project. However, you can also specify another executable project as the start project.
This is how you define the start project:
- In the project explorer, select the node of the project that you want to define as the start project.
- Right-click and select Set as start project from the context menu.
The project name appears in bold in the project explorer. If you press F5, the project is started.