Copy and Paste via the clipboard

It is not always desirable or sensible to have to create hundreds or even thousands of new definitions within the development environment. For this task, the table editor supports an Excel-compatible clipboard format.

A text group from the language switcher can be copied to the clipboard (select the project explorer, then press Ctrl + C) and pasted into Microsoft Excel (open Excel and press Ctrl + V in the first field).

Two tables are inserted here (text groups <Language.Groups> and texts <Language.Texts>), whose structure is very similar to the parameters of the corresponding definitions. The first line below the table identifier in angle brackets shows the parameter names. This is followed by the definition values. The additional [Parent] field establishes the reference to the parent definition.

The reverse method, i.e. copying from Excel and pasting into »EASY UI Designer«, works in the same way, but under the following conditions:

So if you select the existing text group before pasting, a group with the same name is created underneath and the corresponding texts are created in it. If, on the other hand, you select the superordinate node User texts, the system determines that the definitions named in the clipboard already exist in the project and asks what to do. You can then choose whether you want to overwrite the definition parameters in the project with the values from the clipboard.

If, for example, you select the Variables node with the clipboard content specified here and paste it there, nothing happens because the content of the clipboard is pre-filtered using the table identifiers placed in angle brackets.

If you stick to the predefined table template in Excel, you can customise your own lists accordingly and copy them to the project via the clipboard.

Parameter assignment

Sequence when inserting