Create and set up a new project

When you start »EASY UI Designer«, the project configurator is displayed first. By selecting New projecton the start page, you are taken to a page where you can create a completely new project (+) or create a project based on an already saved template.

Create project

To start creating a customised project, click on the plus sign(+). An empty project can be created using the right mouse button and the empty selection. In the latter case, only the absolutely necessary settings are configured.

Alternatively, you can also create a project based on a template you have created yourself under Custom templates.

After you have created a new project on the start page using the plus sign(+), you will be guided through various dialogues to define the project settings.

Set up project