Rights
When scanning the project, the cross-reference searches for uses of rights in the design area of the client project, e.g. in the "Authorisation right" property of the controls. For each use, the cross-reference checks whether the respective right has been defined and, conversely, whether a defined right has been used.
After scanning the project, the results are displayed in a table in the "Rights" view in the cross-reference node.
The table contains the following columns:
Law
Specifies the name of the right.
Status
Indicates the status of use: "Correct", "Warning" or "Error".
Detailed information on the status.
|
Status Description |
Description of the |
Status |
|---|---|---|
|
Correct |
The use of the definition is error-free. |
Correct |
|
Defined, but no use found |
The right has been defined but not used. Important: If the cross-reference is not used for a right, this may have the following reasons:
|
Warning |
|
Used, but not defined |
The right was used, but no definition of this right was found. The control element in which this right is used is not enabled at runtime. |
Error |
System
The entry "Design" means that the definition is used in the design area.
Used in
Specifies the relative path of the page where the right is used.
Source group, source, source detail
Further details on use.