Add an existing view, page or dialog

You can add your own content to the project via the project explorer.

  • To add an existing HTML file as a page, view or dialog:

  1. Expand the [Project]_ClientWDesign folder.

  2. Depending on whether the HTML file is to be added as a page, view or dialog: Right-click on the corresponding subfolder (Pages, Views, dialogs) to open its context menu.

  3. Select the Add existing element command in the context menu.

  4. Select the HTML file to be added in the selection dialog.

  5. Click on the Open button to add the HTML file to the project.