Layout

Three layout types are offered for the main view AppShell.html at »EASY UI Designer«.

FixClassical

The FixClassical layout has a header and a series of navigation buttons at the bottom of the screen that can be used to call up the various pages of the machine visualisation. Elements can only be positioned absolutely, so this layout is only suitable for display sizes with a similar resolution.

FixTop

The FixTop layout has a header containing all buttons for navigation and settings. Elements can only be positioned absolutely, so this layout is only suitable for display sizes with a similar resolution.

Responsive

The responsive layout is suitable for displaying visualisations on very different client devices (e.g. desktop PC and smartphone). Due to the logic required for this, elements in this layout cannot be positioned absolutely. The menu can be flexibly expanded and collapsed using a burger icon.