Changing the order of menu items

  • To change the order of the menu items:

  1. If you have not already done so, open the main view "AppShell.html" in the Designer workspace.

  2. To change the order of the main elements, select the AppNavMenu element in the document structure. To change the order of submenu items, select the corresponding submenu element in the document structure instead.

  3. In the properties window under MenuWMenu Items (Collection), click on the button .

    The Collection Editor dialogue box is displayed:

  4. Make the desired adjustments.

    1. You can use the buttons and to change the position of the selected element within the menu.

    2. You can add a menu item using the Add button. Under NavigationWPageName, you can select the target page that should be displayed when the menu item is selected.

    3. Under TextWLocalizableText, you can assign a text that can be switched in the language to the menu entry.

  5. Click the OK button to apply the changes.