Delete project from target system

You can delete projects from target systems using the Server Manager.

  1. Open the Target Device Manager in the IDE by selecting Project > Target Device Manager in the ribbon.

  2. Type the IP address in the Host field and press Enter to connect to the target device.

  3. If connecting to the target device is successful, open the Server Manager by clicking the blue symbol next to the settings.

  4. A new window appears, in which all client and server projects residing on the target device are listed.

  5. Select the corresponding entry and delete the project by clicking the DELETE button located at the bottom right of the project overview.

  6. In the dialog that opens, confirm the action by clicking DELETE.

    If you want to remove the entire project from the target system, delete both the client and the server project.