Parameter links between alarm definition and alarm type
Alarm types are templates for alarms and contain some of the same parameters as alarms, e.g. alarm class, text, priority, etc. You can specify whether the parameter of the alarm type definition or the corresponding parameter of the alarm definition should apply or whether the values of both parameters should be added together. For text parameters, you can also combine texts from both definitions into one text using the @J@ formatting instruction (for an example, see Example: Alarm type bit block).