Configuration of the runtime behaviour

The configuration of the runtime behaviour is carried out in the "Advanced" tab.

The following settings are possible:

Alarm system only sets 1 bit in the associated status variable (alarm has been acknowledged)

Resetting the acknowledgement variables

Determines whether the alarm server automatically resets the acknowledgement variable after the alarm status change.

Priority of the system alarms

Defines the priority of system alarms. System alarms are triggered by the VisiWin server applications. They include, for example, communication faults.