The project explorer node allows system-wide settings of the recipe server. The configuration is carried out in the Property pages window.
The following settings are available:
-
file format
- Defines the format of the recipe file:
- XML
- A VisiWin-specific XML format.
- MS Access
- Microsoft Access2000 database.
- Only affects
standard server
- Sort mode
- The parameter defines for all recipe classes how the recipe elements are sorted when called up via the recipe class object.
-
- None
- The list of recipe elements does not have a fixed order.
- Sort index
- The recipe elements are sorted numerically in ascending order according to their sort index parameter.
- Variable name
- The recipe elements are sorted alphabetically in ascending order according to their Variable parameter.
- Number of simultaneous orders
- Defines the number of orders that the recipe server can buffer. A job is the request for a transfer function (loading, saving, reading or writing a recipe). The requests from transfer functions are buffered and processed one after the other.
- Only affects
standard server