Sort recipe elements (dialogue)

Dialogue for convenient sorting of recipe elements.

Current sorting
The list shows the current sorting of the recipe elements.
New sorting
The list shows the desired new sorting of the variables. This sorting is accepted by clicking OK.
Tip: If not all variables have been transferred from the left-hand list, they are automatically appended to the right-hand list when closing.
These buttons can be used to move selected variables from one list to the other.
These buttons can be used to move selected variables up or down within the right-hand list.
Select
Clicking on an element changes the selection status. If the Ctrl key is pressed at the same time, a multiple selection can be achieved. Dragging a rectangle with the mouse selects the elements.
Filters
The Filter text field can be used to filter the list on the left by sub-terms in order to find specific variables more quickly.