Project file
Full name of the project file (*.vw7).
The project file contains the localizable texts, which can be structured with hierarchical text groups. Each text and each text group is identified by a name. These names are exported to the target files and later serve as a key when importing in order to establish an assignment between the project text and the translated text. A text to be displayed for each project language is saved in the project file for each localizable text definition.