Return values (translation manager)

When the programme is called via the command line, the programme returns the following values in the %ERRORLEVEL%variable:

Value Description of the
0 No errors have occurred. All texts were successfully exported or imported.
1

Warnings:

  • The programme starts, but ignores some arguments as they do not match the project. The ignored arguments are logged.
  • Some texts were not exported or imported, or possibly not completely. The texts are logged with the cause.
2

Error:

  • The programme cannot start because arguments were specified incorrectly. The incorrect arguments are logged.
  • Some texts were not exported or imported. The texts are logged with the cause.
3 An unexpected programme error has occurred. The programme aborts during the programme run.
4 The log file (LogFile) could not be opened. The programme terminates immediately.