Language selection dialogue
To import texts, the files containing the texts to be imported must be specified. It can happen that the target language is no longer saved in the import file. This sometimes happens with Xliff files that are written by external translation tools. The translation manager then tries to determine the target language based on the file name. If this is also not possible, the user is asked which language the import file contains.
| Setting | Description of the |
|---|---|
| OK | The target language must first be selected from the list. |
| Cancel | The target language cannot be recognised. The file is then ignored for the import. |