Select text groups

In VisiWin, localizable texts are managed in hierarchically organised text groups. When exporting, only a sub-area of this hierarchy can be exported in order to assign a sub-area to a specific translator.

A tick in front of a text group means that only the texts of exactly this selected text group will be exported. It does not indicate that the subgroups are also selected! If some subgroups are marked differently, this is indicated behind the group name with the symbol n and a tooltip. If this symbol is not displayed, the selection (tick/no tick) of the text group is identical to all subgroups.

Tree view

Clicking on a text group selects or deselects this group including the subgroups. If only this one text group is to be edited, the Ctrl key must be pressed at the same time as the mouse click. The space bar can also be pressed instead of a mouse click. This then affects the selected text group.

Selects all text groups including their subgroups.

Deselects all text groups including their subgroups.