MC_GearOut

This FB serves to cancel again the synchronous motion between master and slave axis established with the FB MC_GearIn .

  • The slave axis is accelerated to a constant velocity.
  • As long as the FB is active, it provides setpoints.

 

 

 

MC_GearOut

 

 

 

AXIS_REF

-

Slave

Done

-

BOOL

BOOL

-

Execute

Busy

-

BOOL

Error

-

BOOL

ErrorID

-

L_IE1P_Error

 

 

 

 

 

 

 

 

Inputs

Name

Data type

Information/possible settings

Slave

AXIS_REF

Transfer of the axis data structure of the slave axis

Motion axes (AXIS_REF)

Execute

BOOL

FALSE รค TRUE

Cancel coupling of the slave axis to the master axis.

Outputs

Name

Data type

Value/meaning

Busy

BOOL

TRUE

Processing is running.

Done

BOOL

TRUE

Coupling of the slave axis to the master axis is cancelled.

Error

BOOL

TRUE

An error has occurred. For details see ErrorID .

ErrorID

L_IE1P_Error

If Error = TRUE: Error number for the error that has occurred.