MC_RemoveAxisFromGroup

This function block is used to remove an AxisRef from an AxesGroup from within the application.

Tip!

If all drive and auxiliary axes are to be removed from the axis group, the use of the FB MC_UngroupAllAxes is recommended.

Note!

An axis group can only be activated and used once all required ACS axes have been assigned to the axis group. The virtual Cartesian axes (WCS axes) are always permanently linked to the axis group and cannot be removed, nor can additional WCS axes be added.

Note!

An axis can only be assigned to or removed from an axis group if both the axis is in the Disabled state and the axis group is in the GroupDisabled state.

 

 

 

MC_RemoveAxisFromGroup

 

 

 

AXES_GROUP_KIN

-

AxesGroup

Done

-

BOOL

BOOL

-

Execute

Busy

-

BOOL

IDENT_IN_GROUP_REF

-

IdentInGroup

Error

-

BOOL

     

 

ErrorID

-

L_IE1P_Error

 

 

 

 

 

 

 

 

Inputs

Name

Datentyp

Information/possible settings

AxesGroup

AXES_GROUP_KIN

Axis group reference

Axis group from which an axis is to be withdrawn

Execute

BOOL

FALSE ä TRUE

Start execution of the FB

IdentInGroup

IDENT_IN_GROUP_REF

Selection of the kinematic ACS axis to be removed from the AxesGroup.

  • 7: A1
  • 8: A2
  • …
  • 12: A6
  • 13: Aux1
  • ...
  • 18: Aux6
Outputs

Name

Datentyp

Value/meaning

Done

BOOL

TRUE

The axis was successfully removed from the axis group

Busy

BOOL

TRUE

Processing in progress.

Error

BOOL

TRUE

An error has occurred. For details see ErrorID .

ErrorID

L_IE1P_Error

When Error = TRUE: Error number for the error that has occurred.

Reference manual "FAST technology modules":

Here you will find information on error or warning messages.