MC_TrackRotaryTable
This FB can be used to synchronize a kinematic system with a rotary table. This makes it possible to pick up or place workpieces synchronized from a moving rotary table. For this purpose, the FB calculates a dynamic Product Coordinate System (PCS) after the call. If a motion-guiding FB (e.g. MC_MoveLinearAbsolute ) is called in the same coordinate system, the FB synchronizes the movement with the moving PCS.
|
Note!
The AXIS_REF RotaryTable at the input of the function block must be configured so that a full rotation of the rotary table is displayed as 360Units = 360°. |
|
Note!
Synchronization with a rotary table is only possible with Cartesian movement commands (e.g. MC_MoveLinearAbsolute, MC_MoveCircularAbsolute, ...). Single-axis commands or MC_MoveDirect movements cannot be combined with tracking.. |
|
|
|
|
MC_TrackRotaryTable |
|
|
|
|
|---|---|---|---|---|---|---|---|
|
AXES_GROUP_KIN |
- |
AxesGroup |
Done |
- |
BOOL |
||
|
AXES_REF |
- |
RotaryTable |
Busy |
- |
BOOL |
||
|
BOOL |
- |
Execute |
Active |
- |
BOOL |
||
|
BOOL |
- |
Abort |
CommandAborted |
- |
BOOL |
||
|
ARRAY[1..12] OF LREAL |
- |
RotaryTableOrigin |
Error |
- |
BOOL |
||
|
ARRAY[1..12] OF LREAL |
- |
InitialObjectPosition |
ErrorID |
- |
L_IE1P_Error |
||
|
L_MC4P_CoordSystem |
- |
CoordSystem |
InSync |
- |
BOOL |
||
|
L_MC4P_CoordType |
- |
CoordType |
DynPCSSet |
- |
BOOL |
||
|
LREAL |
- |
ClutchDistance |
|||||
|
LREAL |
- |
ClutchTime |
|||||
|
LREAL |
- |
ClutchTimeAbort |
|||||
|
BOOL |
- |
SetDynPCS |
|||||
|
|
|
|
|
|
|
|
|
Input
|
Name Data type |
Information/possible settings |
|
|---|---|---|
|
AxesGroup AXES_GROUP_KIN |
Axis group reference |
|
|
RotaryTable AXIS_REF |
Axis reference |
|
|
Execute BOOL |
FALSE ä TRUE |
Start processing: Monitor the movement of the rotary table cyclically and wait for the start of a movement in the CoordSystem coordinate system |
|
Abort BOOL |
FALSE ä TRUE |
The current processing is canceled and the axle group is disengaged. To disengage, the time specified at input ClutchTimeAbort input is used for disengagement. |
|
RotaryTableOrigin ARRAY [1..6] OF LREAL |
Position and alignment of the Rotary Table coordinate system from the perspective of the WCS. |
|
|
InitialObjectPosition ARRAY [1..6] OF LREAL |
Position and orientation of the dynamic PCS at the time Execute = FALSE ä TRUE
|
|
|
CoordSystem |
Select the PCS coordinate system to be used:
|
|
|
CoordType |
Type of PCS to be generated:
|
|
|
ClutchDistance LREAL |
Coupling and decoupling distance in [units]
|
|
|
ClutchTime LREAL |
Coupling and decoupling time in [s] Time until engagement and disengagement is complete. |
|
|
ClutchTimeAbort LREAL |
Decoupling time in [s]
Note: If no value is entered, i.e ClutchTimeAbort = 0, the value from ClutchTime is adopted. |
|
|
SetDynPCS BOOL |
FALSE ä TRUE |
Opposite to the Execute delayed setting of the PCS. See section Delayed setting of the PCS |
Outputs
|
Name Data type |
Value/meaning |
|
|---|---|---|
|
Done BOOL |
TRUE |
Processing successfully completed. |
|
Busy BOOL |
TRUE |
Execution in progress.
|
|
Active BOOL |
TRUE |
The FB is currently being executed and superimposes a movement instructed by MC_Move... . |
|
CommandAborted BOOL |
TRUE |
The command was interrupted by another FB or the Abort input. |
|
Error BOOL |
TRUE |
An error has occurred. For details see ErrorID . |
|
ErrorID |
If Error = TRUE: Error number for the error that has occurred. |
|
|
InSync BOOL |
TRUE |
Kinematics move synchronously with the conveyor belt. |
|
DynPCSSet BOOL |
TRUE |
Dynamic PCS is set and can be used. |