The file menu provides functions for creating, managing, editing or importing projects.
The File menu opens as soon as you have started the development environment.
The following functions are available in the menu:
Creates a new project using the project wizard.
In the Recently used projects list, projects that have already been loaded are displayed in chronological order. The newer projects are sorted at the top, the older ones further down. The list contains a maximum of 100 projects. Older projects are not displayed. The list of projects can be deleted using the 'Delete recently used projects' function in the Options dialogue.
Imports and converts a VisiWinNET project of version 6.5 into the current EASY UI Designer version.
The steps for a successful conversion are explained in the chapter .
Terminates the execution of the development environment. EASY UI Designer is closed.
As soon as you have opened a project in the development environment, the File menu also contains the following functions: