Dialog options (IDE)

In the Options dialog of the IDE, you can adjust some functionalities of the »EASY UI Designer« development. For example, you can change the language of the user interface or change the storage location for projects.

To open the dialog, select Tools > Options in the ribbon.

Options dialog

On the left pane, the options are organized by subject in a navigation tree. You can expand the individual nodes. Click on a subnode to see the available options on the right pane of the dialog.

  • Some options become effective only after you close and restart the IDE.

  • A very useful feature that you can enable using the Options dialog is the Track active document in the project explorer option (expand Development > Extended).

Development

Global options for the development or for individual components are available under this node.

General

Variable selection dialog

If the "Show filter settings" option is activated, an additional button with a filter symbol is displayed in the Copy variable to clipboard and Select variable dialogs, which opens a dialog for configuring the filter.

Diagnostics

Errors that occur in the development are logged in the "VisiWin7.Development0.log" file. If a project was loaded in the development when the error occurred, the log file can be found in the project folder. If no project was loaded, then in the directory for user settings. If the log file has reached its maximum size, a new one is created with the index 1 (VisiWin7.Development1.log). A maximum of four files can be created (up to VisiWin7.Development3.log), after which the older file is overwritten. The size and number of these log files cannot be configured.

Editors

The table editor can be configured using the options offered.

Extended

Advanced options for the »EASY UI Designer« development can be found here.

Cross reference

Here you can specify that variable and/or text definitions that are not used in the application and are therefore superfluous are listed in the cross-referenceand marked as a warning.

This option can be used to optimise the project file. If too many variables or text definitions have been imported or created, this can lead to problems with the performance of the IDE. The number of variables is limited to 300,000. You can use this option to display the superfluous definitions and delete them if necessary.

Project explorer

Here you can specify which file types are displayed in the project explorer.

Designer

Options for configuring the Designer are available in this area.

Project management

This area contains options for project management.

Project transfer

This area contains options for configuring the transfer of projects to the target system.

Web (HTML5)