Cross reference

The cross-reference checks the project for the use of variables, texts, rights and unit classes and indicates potential errors. In addition to these definition types, bindings can be checked for Modern UI projects and font classes for Classic UI projects.

example: You can use the cross-reference to check your project, for example, to see whether the variables that are linked in the control elements exist in the project file. If this is not the case for a variable, an error is displayed for this variable. You can then "jump" to the source of the error from the cross-reference, correct the variable connection and thus avoid a system error at runtime.

Open editor

The cross-reference can be found in the project explorer as the last entry in the project configuration node of a project. Each project has its own cross reference.

To open the cross-reference editor, you have the following options:

The editor is opened in a tab in the centre of the development environment.

Control elements

The cross-reference editor has the following operating elements:

Figure 1. editor of the cross reference
Tab
A separate editor is opened for each project on a tab in the centre of the program window of the development environment.
Tip: You can, for example, drag a single tab out of the development environment to display it in a separate window or organise tabs into groups. For more information, see Tabs.
Toolbar
Contains the general functions and functions for filtering the results.
View
The scan results are displayed here. There is one view each for bindings, variables, texts, rights, font classes and unit classes. To display the results for variables in the editor, for example, click on the Variables sub-node of the cross-reference in the project explorer.
Search
You can reduce the results list to the results that contain a specific character string within the first column. To do this, type this character string into the search field. The number of hits is displayed in an output field next to the search field.
Show and hide details
The bindings, variables, texts etc. (nodes) found are highlighted in light yellow. You can expand each node by clicking on the plus symbol to display further information, e.g. a more detailed description of the error and where it occurs. You can hide the information by clicking on the minus symbol .
Columns
You can make each column in the table wider or narrower, just like in the table editor, or double-click to make it fit exactly. You can sort the results by clicking on the column header. Detailed information on the results is displayed in the columns.
Status bar
Indicates the time of the last analysis and the number of errors, warnings and correct usages in the table.
Remark:

The filter for warnings is hidden by default for variables and texts in the toolbar. Warnings for variables and texts are also not counted in the status bar. If you want to use the filter for warnings for variables and texts and have the number of warnings displayed in the status bar, you can set this in the Optionsdialogue. To do this, expand the Development environment node in the dialogue, select the Cross reference view and activate the Variable defined but not used and Localised text defined but not used options.

Scan project

If the cross-reference editor is open, select the desired view, e.g. variables below the Cross-reference node in the project explorer and click on the (scan project) or (rescan project) button in the editor toolbar.

The results are displayed in a table.

Figure 2. results for variables

Filter results

The toolbar contains filter functions that filter the results in the table by status.

When you open the cross-reference editor, all filters (except for the Show system texts filter in the Texts view) are initially activated. This means that the list of results is usually quite long. You can filter the results for a systematic check. To do this, click on the desired filter in the toolbar to activate or deactivate it.

example: If you only want to see results with the status Error, for example, leave only the switch activated and deactivate the others.

Sort results

You can sort the displayed data records in ascending or descending order by clicking on the desired column header. A small triangle pointing upwards or downwards in the column header indicates the corresponding sorting (upwards: ascending sorting, downwards: descending sorting).

example: If you want to sort the data records by status, for example, click once on the Status column header. The data records are sorted in the order Correct-Warning-Error (ascending). If you click on the Status column header a second time, the data records are sorted in the order Error-Warning-Correct (descending).
In the Status Description column, you can sort as follows:
  • Ascending:
    • Correct
    • Defined, but no use found
    • Used, but not defined
    • Usage error (bit number)
  • Descending:
    • Usage error (bit number)
    • Used, but not defined
    • Defined, but no usage found
    • Correct
Alphabetical sorting is used in all other columns (ascending: A-Z, 0-9; descending: Z-A, 9-0).

Show details

To examine a data record in more detail, first expand the desired data record by clicking on the plus symbol to display the relevant information. You can also expand all displayed data records at once by clicking on (Open all nodes) in the toolbar. Errors are highlighted in red, warnings in yellow.

Figure 3: All nodes open

In the expanded view, the exact information on a data record is visible in the columns Status Description, System, Used in etc.

example: Variable1 is used in the screenshot above. This is an error because the variable is used in the application ( System column) but is missing in the project file ( Status Description column). Variable1 is used in MainView1.xaml ( Used in column) in the VariableName property ( Source column) of a control of type NumericVarIn ( Source group column).

Navigate to the source

If you have expanded a data record, you can navigate directly to the source of a usage:

If the usage can be found on a form, a view or a page, the corresponding document is opened in the Designer and the usage is selected. If the usage can be found in a definition (e.g. in an alarm), this definition is opened in the table editor and selected.

Remark:Automatic marking in the Modern UI

The view must already be open in the Designer for the relevant control element to be selected automatically. The Show definition command must therefore usually be executed twice: The first time the view is opened in the Designer, the second time the control element is selected.

Figure 4: Use in WPF Designer automatically marked

In the Modern UI, you can also highlight the relevant position in the XAML text. To do this, activate the Xaml view for the view and execute the Show definition command in the cross reference again.

Figure 5: Use in the XAML view of the WPF Designer automatically marked
Restriction: Automatic marking is not (yet) available in the Web UI.

Correct errors and update cross-reference

Once you have corrected the error, e.g. specified the correct variable in the VariableName property of the control, save the document in the Designer and scan the project again to update the cross-reference data.

Tip: You can have documents saved automatically in the Designer. To do this, open the Options dialogue, expand the Designer node in the dialogue, select the Documents view and activate the Automatically save documents option. You can also set the time period after which documents are automatically saved here. Confirm your changes with OK.