Bindings

The cross-reference searches for bindings in the design area of the project and checks whether the source for the binding is available.

Restriction: The binding check is only available in Modern UI (WPF) client or single projects.

After scanning the project, the results are displayed in a table in the Bindings view in the Cross-reference node of the project.

The table contains the following columns:

Binding
Specifies the binding, e.g. {DynamicResource ApplicationBackgroundBrush}.
Status
Indicates the status of use: either Info, Correct or Error.
Status Description
Detailed information on the status.
Status Description Description of the Status
Info The binding cannot be assigned either the status Erroror the status Correct. Info
Correct The use of the binding is error-free. Correct
ResourceKey not available The source of the binding(x:keyor ResourceKey) could not be found. Error
System
Only PropertyBindingis specified as the system.
Used in
Specifies the relative path of the view or resource that contains this binding.
Source group, source, source detail
Further details on use