Drag windows out of the development environment and integrate them again
To create more space in the development environment, you can drag individual windows, e.g. the document to be edited, the properties window, etc., out of the development environment. A window that has been dragged out can be reintegrated into the programme window of the development environment.
Remove the window from the development environment:
-
Left-click on the tab of the desired window, e.g. Properties, and drag it out of the programme window while holding down the mouse button. Release the mouse button at the desired position.
-
You can now adjust the window size if required. The procedure is the same as for enlarging and reducing windows within the programme window of the development environment.
Reintegrate the window into the development environment:
-
Click on the tab of the window and drag it back into the development environment while holding down the mouse button. The procedure is the same as for positioning windowswithin the programme window of the development environment.