PanoramaView

A placeholder control that enables navigation through multiple views.

Symbol

Menu ribbon

Start > Controls > Navigation > Container > PanoramaView

The "PanoramaView" control element contains one or more "PanoramaViewItems", to each of which a view is linked. Two so-called "Indicators", which are shown as arrows in the standard version, can be used to navigate through the various views at runtime. The swipe gesture can also be used for this on touch devices.

Exemplary representation of a PanoramaView with three PanoramaViewItems

Functionalities

The control element supports the following functionality:

Style

The PanoramaView is available in the following styles: Lenze.Default, LenzeCyan.Default, Custom.Default. However, there are no visual differences due to their placeholder function.

Structure and properties of the PanoramaView

The PanoramaView and its elements

The control contains internal containers for displaying the view (PanoramaViewItem), the navigation arrows and the indicator components.

PanoramaView

By default, the PanoramaView contains one PanoramaViewItem. The collection can be supplemented with additional PanoramaViewItems under PanoramaWViews. Visual adjustments are possible for the navigation arrows via the corresponding colour and symbol properties in the "Left Arrow", "Right Arrow" and "Colors" categories. One indicator element is created in the indicator container for each integrated PanoramaViewItem. By default, the frames of the indicators are coloured and rounded so that they provide an overview of the current navigation area as points. However, images or texts can also be displayed for each PanoramaView item. These options can be configured generically under "View Indicators Symbol" or "View Indicators Text", but the specific images or texts must be selected on the corresponding PanoramaView item.

Furthermore, the swipe gesture can be (de)activated on a touch-based end device (Swipe enabled) and the transition time between the views (transition duration, default is 400 ms) can be defined.

PanoramaViewItem

To display a view, it must be linked to the "View" property in a "PanoramaViewItem". The "PanoramaViewItem" can be linked to an icon or text that can be used as a preview for navigation. It is also possible to hide a view using the user rights.

Related topics: