The free parameters are configured on the tab of the same name. Free parameters can be added to or deleted from the project here.
Each parameter contains the following information:
- Name
- The name of the free parameter is shown in the column header in the alarm table.
- Data type
-
The following data types are predefined:
- Int32
- Integer values
- Double
- Floating point numbers
- Text
- Unformatted text
- File
- The binary content of a file with file selection dialogue
- Image
- A picture
- Standard language
- Free parameters can also be managed individually for each project language. Language switching is therefore possible. In cases where language switching of the free parameters is not necessary, the language in which the parameter value is saved can be specified here. The value from the default language is then used as the fallback strategy in all alarms in which the value of the free parameter was not specified in a language.
- Usage figure
- Additional numerical information on the parameter
- Comment
- Freely selectable comment
Subject:
Only
Standard server
Note: In the cross-platform server, the free parameters are replaced by the general system of pinned parameters.