Unit text

Specifies an additional text that is transferred to the display controls at runtime and describes the physical size of the unit.

If the unit text begins with an @ character, the value is interpreted as the identifier of a localizable text. The corresponding text in the language currently set in the application is then returned in the display. Assigning a language-dependent unit text is useful if a unit is to be switched via a variable and the textual specification is also language-dependent.

The text configured here has no functions in the unit conversion between the variable server and the communication component (unit class (process)).

Parameters for module: