Definition: Unit objects

Unit definitions represent the switching options of a unit class. The key information here is the formula for conversion and the specification of the state (language or process variable value) that must be assumed for the formula to become active.

Unit objects include the following functionality, among others:

Parameter name

Description of the

Unit text

Additional text to be transferred that is to be displayed in the visualisation

Decimal point shift

Shifting of integer values by decimal places.

Switching identifier

Describes the status so that this unit is used as a conversion in the unit class.

X1

Describes the 1st raw value of the linear equation.

X2

Describes the 2nd raw value of the linear equation.

Y1

Describes the 1st conversion value of the linear equation.

Y2

Describes the 2nd conversion value of the linear equation.