Definition: Unit class

Unit classes enable the variable-value or language-dependent conversion of process variables by the variable server. The reference of a process variable to a unit class is established by the parameters unit class (process)/(display). The conversion can take place at two points in time.

Unit classes include the following functionality:

  • A language-dependent unit class cannot be used in the unit class (process) parameter of a process variable.

  • If a variable-dependent unit class is specified in the Unit class (display) parameter of a process variable, it almost always makes sense in a client-server system to mark the switching variable of the unit class as "client-internal" (see Variable options parameter).

Parameters

Unit class (variable-dependent)

Name

Description of the

Comment

Optional commentary on the object.

Name

Name of the object.

Switchover variable (unit class)

Variable for switching between the unit objects

Unit class (language-dependent)

Name

Description of the

Comment

Optional commentary on the object.

Name

Name of the object.

Standard language

Defines the unit to be used if no unit object has been defined for the current language.