Automatically write recipe buffer to the variable server when changes are made

Previously: Write changed values directly

The parameter causes values changed via the application (e.g. in the VisiWin control elements) to be sent directly to the PLC via the variable server, i.e. without triggering the Write trigger function.

Parameters for

Recipes module:
Recipe class

See also