Automatically save recipe buffer in current recipe file when changes are made
Previously: Save changed values directly
The parameter causes values changed in the recipe buffer via the application (e.g. in the VisiWin control elements) to be written directly to the current recipe file via the recipe server, i.e. without triggering the Save trigger function.
Note: The changed process values are written to the last recipe file used. In order for the values to be saved, the Load or Save function must have been executed at least once beforehand or the initial recipe name must be specified in the recipe class definition.
Parameters for
- Recipes module:
- Recipe class