Variable for read trigger
Defines a variable whose value change to 1 triggers the reading of values from the variable server into the recipe server. After reading, the value of the variable is automatically reset to 0. The variable can have either a Boolean or an integer data type. The bit serving as the trigger is then selected by specifying the bit number in the variable selection dialogue.
Parameters for
- Recipes module:
- Recipe class