Read access
Determines whether read access to process variables in this group of the communication component should be synchronous or asynchronous.
|
Setting |
Description of the |
|---|---|
|
Synchronisation |
The variable server forwards a read request to the communication component and waits until the process variable value is returned. Synchronous reading increases data consistency in the variable server, as there is always a wait after the request until the process variable value is returned. A disadvantage, however, is that the entire system may have to wait for the process variable value to be returned if the communication component does not return the data quickly enough. |
|
Asynchronous |
The variable server sends a request to read a process variable value to the communication component. After processing the read request, the communication component sends a message containing the process variable value to the variable server. The advantage is that the variable server continues to work between the request and the message. |
For process variables from VisiWin drivers, this setting only has a function if the Enable synchronous communication parameter is activated. Otherwise, the variable requests are executed asynchronously.
Parameters for module: