Definition: Group

Group definitions are used to control data exchange: process variables from different communication channels can be assigned to a group. The group definition contains the information in which cycle or for which event the process variable values are exchanged between the variable server and the communication component.

For the data exchange to work at all, each process variable must exist in a group. Therefore, all new process variables added to a project are automatically entered in the "Standard" group.

Groups provide the following functionalities:

Parameter name

Description of the

Sampling time

Cycle time of the data exchange

Definition active

Determines whether the object definition is valid.

Activation mode

Data exchange automatically or controlled by variable value

Hysteresis

Degree of change of process variable values at which a read access is triggered.

Comment

Optional commentary on the object.

Read access

Synchronous or asynchronous data exchange for read access.

Name

Name of the object.

Write accesses

Synchronous or asynchronous data exchange for write accesses

Trigger variable

Process variable for controlling the reading and writing of a group

Time zone difference

Correction of the process variable timestamp when a time zone limit is exceeded