Definition active

Determines whether the object definition is valid. If the parameter is deactivated, the object definition is ignored by the runtime system when the programme is started. The corresponding object then does not exist.

Tip: You can use this parameter to "hide" object definitions that are not yet fully configured when testing your project.
Important: This parameter must not be confused with the parameters Communication active and Active at runtime.