Definition: Assignment

Within an alarm type definition, an assignment establishes the relationship between a value (for the "Numeric" alarm type) or a bit (for the "Bit block" alarm type) and the data of a simplified alarm definition. This naturally includes an alarm text, but also the priority, the reference to an alarm class and other parameters.

This data is used at runtime by the alarm definition that uses the associated alarm type. Depending on the configuration in the alarm type, only the data of the assignment is used or it is mixed with the data of the alarm definition.

Parameter name

Description

0-active

Alarm type bit block only

Alarm is triggered when the corresponding bit is set or reset.

Alarm class

Reference to the alarm class that defines the appearance and other functions of the alarm.

Bit number (Alarms module)

Alarm type bit block only

Defines the bit within the variable that triggers the function.

Bit number (Alarms module)

State variable

Defines the bit within the variable that triggers the function.

Bit number (Alarms module)

Acknowledgement variable

Defines the bit within the variable that triggers the function.

Definition active

Determines whether the object definition is valid.

Comment

Optional commentary on the object.

Name

Name of the object.

Parameter 1

Any text that provides additional information about the alarm

Parameter 2

Any number (e.g. unique alarm number) that provides additional information about the alarm

Priority

Determines the importance of an alarm.

Acknowledgement variable

Name of the variable with which an alarm can be acknowledged

Status variable

Name of the variable with which the status and the acknowledgement status can be determined

Text

Localisable text for the object.

Value

Numeric alarm type only

Value that must be accepted by the event variable in the alarm definition for this alarm to become active