Priority
The priority is intended to characterise the importance of an alarm. The higher the value, the more important the alarm is. The value can be in the range 0 to231-1(=2,147,483,647).
In the control element, the priority is used to find and display the most important alarm if several alarms are pending at the same time. Alarms can be filtered by priority in the and controls.
Parameters for module: