Definition: Alarm

Alarms are edited in the table editor. They include the following functionality:

Parameter name

Description of the

0-active

Alarm is triggered when the corresponding bit is set or reset.

Alarm class

Reference to the alarm class that defines the appearance and other functions of the alarm.

Bit number (Alarms module) Event variable

Defines the bit within the variable that triggers the function.

Bit number (Alarms module) Acknowledgement variable

Defines the bit within the variable that triggers the function.

Bit number (Alarms module) Status variable

Defines the bit within the variable that triggers the function.

Definition active

Determines whether the object definition is valid.

Event variable

Defines the name of the variable that triggers the alarm

Comment

Optional commentary on the object.

Name

Name of the object.

Parameter 1

Any text that provides additional information about the alarm

Parameter 2

Any number (e.g. unique alarm number) that provides additional information about the alarm

Priority

Determines the importance of an alarm.

Acknowledgement variable

Name of the variable with which an alarm can be acknowledged

Status variable

Name of the variable with which the status and the acknowledgement status can be determined

Text

Localisable text for the object.

Type

Specifies the alarm type with which the alarm definition is extended.