Definition: Alarm group

Alarm groups are displayed in the project explorer under the access node of the same name. Their primary task is to group alarm definitions. Alarm groups can be nested hierarchically.

Alarm groups include the following functionality:

The "System alarm" alarm group is automatically created in a project. This defines the behaviour of all system alarms originating from the server applications (e.g. communication error messages). This group cannot be deleted or renamed.

The alarm group definition contains the following parameters:

Parameter name

Description of the

Bit number (Alarms module)

Deactivation variable

Defines the bit within the variable that triggers the function.

Bit number (Alarms module) Acknowledgement variable

Defines the bit within the variable that triggers the function.

Bit number (Alarms module)

Status variable

Defines the bit within the variable that triggers the function.

Deactivation variable

Variable for switching on/off all alarms contained in the group (at runtime)

Definition active

Determines whether the object definition is valid.

Comment

Optional commentary on the object.

Name

Name of the object.

Priority variable

Variable for saving the highest current priority

Acknowledgement variable

Name of the variable with which an alarm can be acknowledged

Status variable

Name of the variable with which the status and the acknowledgement status can be determined

Symbol

Graphic symbol for the display

Text

Localisable text for the object.