Text
Defines a localizable text for an object. The text entered or displayed in the development environment refers to the developer language selected in the project.
In the table editor, this developer language is also displayed in the column header of the Text column.
The texts for other languages can be found under the Language switch node. A main node is visible there for each system, under which the associated text definition for an object with all languages is visible.
Example:
For example, if you create a new variable definition, the system automatically creates a text definition for this variable in the Language switch > Variables > <channel name> node in the project explorer.
Parameters for module: