Structural element

Structure elements define the memory cells of a structure definition. The most important information is the data type and the offset within the structure.

Structural elements include the following functionality:

  • Substructuring with the help of the data type
  • Access to data fields
  • Language or variable value-dependent conversion of process variable values(unit classes)

Parameters

Name Description of the
Data type Determines the structure and length of the process variable value.
Unit class (display) Reference to a language or variable-dependent conversion.
Unit class (process) Reference to a variable-dependent conversion.
Replacement value Value that is passed on instead of the true process value
Field size Number of process variables for block-based access.
Variable options Bit-coded settings for the process variable
Comment Optional commentary on the object.
Maximum value settings Optional: Upper limit value (constant or variable) that the process variable may assume for a user input.
Minimum value settings Optional: Lower limit value (constant or variable) that the process variable may assume for a user input.
Name Name of the object.
Serial number Byte offset or sequence number of the element in the structure memory area
Text Localisable text for the object.

See also