Serial number
The order number as byte offset parameter specifies how the order number parameter is interpreted in the structure elements.
The order number parameter specifies the position of the structure element within the structure. Depending on the setting of the order number parameter as a byte offset, the order number specification has the following meaning:
|
Setting ordinal number as byte offset |
Description of the |
|---|---|
|
|
The ordinal number is added to the process variable address as a byte offset in order to access the structure element. |
|
|
The sequence number specifies the order of the structure elements. The byte offset on the structure element is calculated from the length of all structure elements with a lower ordinal number. |
Parameters for module: