Definition: Process variable

Process variables represent process data in the visualisation (values that are provided by the PLC as memory cells). The most important information contained in the process variable definition is the ItemID and the data type of the addressed PLC memory area.

In addition to the pure transfer of process data, a process variable definition supports the following special functions, among others:

Parameter name

Description of the

Address/ItemID

Identifier of the process variables from the communication component.

Alias

Identifier of the object

Data type

Determines the structure and length of the process variable value.

Definition active

Determines whether the object definition is valid.

Unit class (display)

Reference to a language or variable-dependent conversion.

Unit class (process)

Reference to a variable-dependent conversion.

Individually writable

Determines whether the elements of a process variable of a complex data type can be written individually to the communication component.

Replacement value

Value that is passed on instead of the true process value

Substitute value mode

Determines when the replacement value is passed on.

Field size

Number of process variables for block-based access.

Comment

Optional commentary on the object.

Maximum value settings

Optional: Upper limit value (constant or variable) that the process variable may assume for a user input.

Minimum value settings

Optional: Lower limit value (constant or variable) that the process variable may assume for a user input.

OPC UA access rights

Defines whether and how the OPC UA client can access the variables via the OPC UA server.

Text

Localisable text for the object.

Variable options

Bit-coded settings for the process variable

Access type

Read/write authorisation for the process variable

Access path

OPC: Optional hardware-specific data path description for the PLC

OPC UA: The namespace of the variables in the OPC UA server