Access type

Determines whether a process variable can be accessed read/write.

Setting

Description of the

R

The variable server reads process variable values from the communication component. Write access is not permitted.

W

The variable server writes process variable values to the communication component. Read access is not possible.

R/W

Both read and write access is permitted.

1xR/W

During the initialisation phase of the variable server, the process variable value is read in once, after which only write access is possible.

Parameters for module: