Definition: Trend

A trend defines which process variable is to be recorded in which way. A trend must belong to an archive.

Once you have created a trend in an archive, you can define the parameters for the trend either in the table editor or on the properties pages.

The parameters are grouped on the following tabs on the properties pages:

Parameter name

Description of the

Definition active

Determines whether the object definition is valid.

Mode (filter)

Filter method before recording

Depth (filter)

Setting for the Filter parameter

Hysteresis

Recording hysteresis (difference value at which a variable value is recorded)

Mode (hysteresis)

Determines how the value of the hysteresis parameter is interpreted.

Comment

Optional commentary on the object.

Maximum

Recording maximum (variable or constant)

Minimum

Recording minimum (variable or constant)

Name

Name of the object.

Text

Localisable text for the object.

Trend variable

Name of the process variable to be recorded