Minimum

The Maximum and Minimum parameters are used to calculate the hysteresis if the Mode (hysteresis) parameter is set to In per mille of Maximum-Minimum.

The parameter accepts the following inputs:

Type

Description of the

Number

A constant (decimal places are separated from pre-decimal places by a dot, e.g.: 1.234)

Text

The name of another process variable whose current value is archived instead of the actual value. A dialogue for selecting a process variable is opened in the editor via the button.

Parameters for module: