Acknowledgement variable

The VisiWin control element supports the acknowledgement of alarms via mouse and keyboard entries. If the acknowledgement is to be carried out without the help of the control element, the acknowledgement variable can be used to carry out an alarm acknowledgement outside of the alarm control elements. This can be done either on the PLC side or in the programme code.

Parameters for module: