Symbol
In the alarm control elements, it is possible to display two symbols for each alarm:
The first symbol is used to display the alarm status. A freely selectable symbol can be set for each alarm status. The symbols can be set in the alarm class.
The second symbol can represent the source of the alarm. This symbol is configured in the alarm group.
The following graphic formats are permitted as symbols: *.bmp, *.ico and *.png.
Parameters for module: