Load last recipe file at start
Defines whether the recipe file last loaded in the last application session should be loaded immediately into the corresponding process variables when the application is started.
After starting the application, the recipe buffer of a recipe class is usually empty. The option described here can be used to initialise the recipe buffer with the last recipe file loaded. Immediately afterwards, the values are automatically transferred to the corresponding process variables and thus to the PLC.
The system remembers the name of the last recipe file opened in the project file between application runs.
Parameters for
- Recipes module:
- Recipe class